ACTION#.CONDITION
Description
This keyword defines the condition to test the action source for. If the value is 0 (always), then no test is performed and the condition always passes.
The available values of this parameter depend on the value of ACTION#.SOURCE. If the source is changed, the available range may be updated and the condition will be reset to default. Available conditions are:
Value | Description |
---|---|
0 | Always passes |
1 | Is false |
2 | Is true |
3 | Less than |
4 | Greater than |
5 | Rising Edge |
6 | Falling Edge |
7 | Rises above threshold |
8 | Falls below threshold |
9 | Rising Edge (triggers on high at start) |
10 | Falling Edge (triggers on low at start) |
11 | Is Equal To |
12 | Becomes Equal To |
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
Depends on ACTION#.SOURCE |
Default Value |
0 (always) |
Data Type |
Integer |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
ACTION1.CONDITION |
3901h |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION2.CONDITION |
3901h |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION3.CONDITION |
3901h |
03h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION4.CONDITION |
3901h |
04h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION5.CONDITION |
3901h |
05h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION6.CONDITION |
3901h |
06h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION7.CONDITION |
3901h |
07h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION8.CONDITION |
3901h |
08h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION9.CONDITION |
3901h |
09h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION10.CONDITION |
3901h |
0ah |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION11.CONDITION |
3901h |
0bh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION12.CONDITION |
3901h |
0ch |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION13.CONDITION |
3901h |
0dh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION14.CONDITION |
3901h |
0eh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION15.CONDITION |
3901h |
0fh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION16.CONDITION |
3901h |
10h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION17.CONDITION |
3901h |
11h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION18.CONDITION |
3901h |
12h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION19.CONDITION |
3901h |
13h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION20.CONDITION |
3901h |
14h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION21.CONDITION |
3901h |
15h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION22.CONDITION |
3901h |
16h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION23.CONDITION |
3901h |
17h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION24.CONDITION |
3901h |
18h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION25.CONDITION |
3901h |
19h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION26.CONDITION |
3901h |
1ah |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION27.CONDITION |
3901h |
1bh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION28.CONDITION |
3901h |
1ch |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION29.CONDITION |
3901h |
1dh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION30.CONDITION |
3901h |
1eh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION31.CONDITION |
3901h |
1fh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION32.CONDITION |
3901h |
20h |
Unsigned8 |
- |
- |
Read/Write |
No |
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
40200 |
1 |
40200 (0x9d08) |
ACTION1.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40201 |
1 |
40201 (0x9d09) |
ACTION2.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40202 |
1 |
40202 (0x9d0a) |
ACTION3.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40203 |
1 |
40203 (0x9d0b) |
ACTION4.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40204 |
1 |
40204 (0x9d0c) |
ACTION5.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40205 |
1 |
40205 (0x9d0d) |
ACTION6.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40206 |
1 |
40206 (0x9d0e) |
ACTION7.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40207 |
1 |
40207 (0x9d0f) |
ACTION8.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40208 |
1 |
40208 (0x9d10) |
ACTION9.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40209 |
1 |
40209 (0x9d11) |
ACTION10.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40210 |
1 |
40210 (0x9d12) |
ACTION11.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40211 |
1 |
40211 (0x9d13) |
ACTION12.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40212 |
1 |
40212 (0x9d14) |
ACTION13.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40213 |
1 |
40213 (0x9d15) |
ACTION14.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40214 |
1 |
40214 (0x9d16) |
ACTION15.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40215 |
1 |
40215 (0x9d17) |
ACTION16.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40216 |
1 |
40216 (0x9d18) |
ACTION17.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40217 |
1 |
40217 (0x9d19) |
ACTION18.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40218 |
1 |
40218 (0x9d1a) |
ACTION19.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40219 |
1 |
40219 (0x9d1b) |
ACTION20.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40220 |
1 |
40220 (0x9d1c) |
ACTION21.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40221 |
1 |
40221 (0x9d1d) |
ACTION22.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40222 |
1 |
40222 (0x9d1e) |
ACTION23.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40223 |
1 |
40223 (0x9d1f) |
ACTION24.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40224 |
1 |
40224 (0x9d20) |
ACTION25.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40225 |
1 |
40225 (0x9d21) |
ACTION26.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40226 |
1 |
40226 (0x9d22) |
ACTION27.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40227 |
1 |
40227 (0x9d23) |
ACTION28.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40228 |
1 |
40228 (0x9d24) |
ACTION29.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40229 |
1 |
40229 (0x9d25) |
ACTION30.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40230 |
1 |
40230 (0x9d26) |
ACTION31.CONDITION |
Unsigned8 |
Read/Write |
Yes |
40231 |
1 |
40231 (0x9d27) |
ACTION32.CONDITION |
Unsigned8 |
Read/Write |
Yes |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
ACTION1.CONDITION |
40200 |
Unsigned8 |
Read/Write |
- |
ACTION2.CONDITION |
40201 |
Unsigned8 |
Read/Write |
- |
ACTION3.CONDITION |
40202 |
Unsigned8 |
Read/Write |
- |
ACTION4.CONDITION |
40203 |
Unsigned8 |
Read/Write |
- |
ACTION5.CONDITION |
40204 |
Unsigned8 |
Read/Write |
- |
ACTION6.CONDITION |
40205 |
Unsigned8 |
Read/Write |
- |
ACTION7.CONDITION |
40206 |
Unsigned8 |
Read/Write |
- |
ACTION8.CONDITION |
40207 |
Unsigned8 |
Read/Write |
- |
ACTION9.CONDITION |
40208 |
Unsigned8 |
Read/Write |
- |
ACTION10.CONDITION |
40209 |
Unsigned8 |
Read/Write |
- |
ACTION11.CONDITION |
40210 |
Unsigned8 |
Read/Write |
- |
ACTION12.CONDITION |
40211 |
Unsigned8 |
Read/Write |
- |
ACTION13.CONDITION |
40212 |
Unsigned8 |
Read/Write |
- |
ACTION14.CONDITION |
40213 |
Unsigned8 |
Read/Write |
- |
ACTION15.CONDITION |
40214 |
Unsigned8 |
Read/Write |
- |
ACTION16.CONDITION |
40215 |
Unsigned8 |
Read/Write |
- |
ACTION17.CONDITION |
40216 |
Unsigned8 |
Read/Write |
- |
ACTION18.CONDITION |
40217 |
Unsigned8 |
Read/Write |
- |
ACTION19.CONDITION |
40218 |
Unsigned8 |
Read/Write |
- |
ACTION20.CONDITION |
40219 |
Unsigned8 |
Read/Write |
- |
ACTION21.CONDITION |
40220 |
Unsigned8 |
Read/Write |
- |
ACTION22.CONDITION |
40221 |
Unsigned8 |
Read/Write |
- |
ACTION23.CONDITION |
40222 |
Unsigned8 |
Read/Write |
- |
ACTION24.CONDITION |
40223 |
Unsigned8 |
Read/Write |
- |
ACTION25.CONDITION |
40224 |
Unsigned8 |
Read/Write |
- |
ACTION26.CONDITION |
40225 |
Unsigned8 |
Read/Write |
- |
ACTION27.CONDITION |
40226 |
Unsigned8 |
Read/Write |
- |
ACTION28.CONDITION |
40227 |
Unsigned8 |
Read/Write |
- |
ACTION29.CONDITION |
40228 |
Unsigned8 |
Read/Write |
- |
ACTION30.CONDITION |
40229 |
Unsigned8 |
Read/Write |
- |
ACTION31.CONDITION |
40230 |
Unsigned8 |
Read/Write |
- |
ACTION32.CONDITION |
40231 |
Unsigned8 |
Read/Write |
- |